41520members
184569posts

Differences between ViewX license and floating license

Highlighted
Crewman

Differences between ViewX license and floating license

I have posted in the other forum regarding my inquiry about the differences between the ViewX license and floating license here.

 

However, I still have further inquiries regarding to what privileges does a ViewX license have compared to the floating license. Like, if I use another workstation to connect to the server holding the floating license, is the workstation able to develop and have complete access and control? And is the ViewX license allowed to be installed on the same server but is used by another workstation connected to the server?

 

Looking forward for your replies.

 

Thank you so much!

1 REPLY 1
Highlighted
Commander

Re: Differences between ViewX license and floating license

Have you already seen this link?

https://www.se.com/ww/en/faqs/FA299727/

 

A ViewX license is a ViewX license, there are not different versions with different permissions.

Once you have a license, you can 'view', 'control', or 'configure' the ClearSCADA database so far as the internal database security permissions allow you to.


Lead Control Systems Engineer for Alliance Automation (VIC).
All opinions are my own and do not represent the opinions or policies of my employer, or of my cat..