I'm looking to determine what version/release of DNP3 and Secure Key Authentication is implemented in ClearSCADA 2017R2 and R3 and 2019. We are researching alternative field equipment and need to know what CS/GS will support.
Thanks in advance for any assistance!
Solved! Go to Solution.
All versions support IEEE 1815-2012 (the current DNP3 standard) however that doesn't really tell you very much as most features in the DNP standard are optional.
All versions support DNP Secure Authentication version 2 (SAv2)
You really want to look at the DNP device profile to get detailed information on what features and options are supported. The device profiles are installed into the "C:\Program Files\Schneider Electric\ClearSCADA\InteropDocuments" folder by default.
See "Geo SCADA Expert DNP Master Device Profile.xml" or "ClearSCADA DNP Master Device Profile.xml".
All versions support IEEE 1815-2012 (the current DNP3 standard) however that doesn't really tell you very much as most features in the DNP standard are optional.
All versions support DNP Secure Authentication version 2 (SAv2)
You really want to look at the DNP device profile to get detailed information on what features and options are supported. The device profiles are installed into the "C:\Program Files\Schneider Electric\ClearSCADA\InteropDocuments" folder by default.
See "Geo SCADA Expert DNP Master Device Profile.xml" or "ClearSCADA DNP Master Device Profile.xml".
Thanks for the reply Andrew!
Appreciate the info.
Discuss challenges in energy and automation with 30,000+ experts and peers.
Find answers in 10,000+ support articles to help solve your product and business challenges.
Find peer based solutions to your questions. Provide answers for fellow community members!