Hi,
Is there a way to add a menu option to the map context sensitive menu in the same way that can be added to the alarm banner context-sensitive menu?
The scripting guide explains the process to add a menu using the function "AlarmBanner.AddMenuItem".
What is the function to add the custom menu?
Thanks for your help
I don't believe there is an easy way to add a Menu Option on the map. Although I haven't tried this exactly.
The Alarm Banner is the most flexible with the scripting capability. It is also possible to add Context Menu options in general locations, but these are more restricted to just additional data queries
It seems my screenshot copy-paste isn't working in this forum today. But I've attached a screenshot showing where such an additional data query could be added.. and the kind of thing that it would be for.
I'd recommend having a look through the current 'Feature Request' list to see if the item you want is already there.. and if so add your vote and potentially add your comment to ensure that your particular use case is documented alongside the existing request.
https://community.exchange.se.com/t5/Geo-SCADA-Expert-Ideas/idb-p/geo-scada-expert-ideas
User | Count |
---|---|
188 | |
56 | |
17 | |
17 | |
16 | |
10 |
Discuss challenges in energy and automation with 30,000+ experts and peers.
Find answers in 10,000+ support articles to help solve your product and business challenges.
Find peer based solutions to your questions. Provide answers for fellow community members!