Create your free account or log in to subscribe to the forum - and gain access to more than 10,000+ support articles along with insights from experts and peers.
Already have an account? Login
You can subscribe to this forum after you log in or create your free account..
Create your free account or log in to subscribe to the forum - and gain access to more than 10,000+ support articles along with insights from experts and peers.
Already have an account? Login
Posted: 2021-03-11 01:18 AM . Last Modified: 2021-03-17 03:48 AM
Dear All,
I bought M700-SRSU.I installed on VGS211F. Stem down is fully close for VGS211.but the M700-SRSU is stem-up fully close.How can I change spring return direction.I want to convert it from SRSU to SRSD.
Posted: 2021-03-11 09:48 PM . Last Modified: 2021-03-11 09:48 PM
I don't believe that this is possible, the spring function is mechanical and cannot be altered. You should return the actuator and purchase the M700-SRSD
Posted: 2021-03-11 09:48 PM . Last Modified: 2021-03-11 09:48 PM
I don't believe that this is possible, the spring function is mechanical and cannot be altered. You should return the actuator and purchase the M700-SRSD
Posted: 2021-03-11 09:52 PM
Ok.thank you for your reply
Posted: 2021-03-12 06:08 AM
Correct Craig, it is not possible to convert an SRU to and SRD
Posted: 2022-02-28 02:16 AM
The M700 SR actuator is also the replacement to the AL..S series actuator from Satchwell along with the L7SV linkage kit for the Satchwell valves listed. As ever, attention is to be paid on selection to which direction the spring is set up to drive upon power failure, the actuator cannot be converted.
User | Count |
---|---|
9 | |
6 | |
4 | |
2 | |
2 | |
2 |
Create your free account or log in to subscribe to the forum - and gain access to more than 10,000+ support articles along with insights from experts and peers.