Invite a Co-worker
Send a co-worker an invite to the Exchange portal.Just enter their email address and we’ll connect them to register. After joining, they will belong to the same company.
Send Invite Cancel
80907members
347028posts

Berapakah maximum Drop Voltage pada instalasi listrik?

Solved
BudiThamrin
Crewman
Crewman
0 Likes
4
189

Berapakah maximum Drop Voltage pada instalasi listrik?

Siang, mau tanya, maximum Drop Voltage pada instalasi listrik itu berapa ya? Terima kasih.

Tags (1)

Accepted Solutions
HelvinHermanT
Captain Captain
Captain

Re: Berapakah maximum Drop Voltage pada instalasi listrik?

Selamat Siang juga,

 

Terima kasih atas pertanyaannya.

 

Rekomendasi maximum Drop Voltage dalam instalasi diatur dalam IEC 60364-5-52:2009 Low-voltage electrical installations – Part 5-52: Selection and erection of electrical equipment – Wiring systems

 

Bisa dilihat dalam Annex / Lampiran G mengenai "Volrtage drop in customers installations". Nilai maximum drop voltage adalah 3 - 8 % tergantung tipe instalasinya dan peruntukannya (Penerangan atau lain lain). 

 

Contoh :

Maximum drop voltage sebesar 3% untuk Penerangan (Lighting) jika disuplai dari Distribusi Listrik Umum tegangan rendah (PLN) dan maximum 6% untuk penerangan dengan suplai dari distribusi listrik tegangan rendah Privat.

Untuk penggunaan lainnya (selain penerangan) maximum drop voltage 5-8% untuk Distribusi Umum dan Private.

 

Dimungkinkan drop voltage lebih besar saat starting motor atau gawai dengan inrush current besar.

 

Voltage Drop Formula.jpg

 

See Answer In Context

Tags (1)
HelvinHermanT
Captain Captain
Captain
0 Likes
1
168

Re: Berapakah maximum Drop Voltage pada instalasi listrik?

 

u is the voltage drop in volts;
b is the coefficient equal to 1 for three-phases circuits, and equal to 2 for single-phasecircuits;


NOTE 3 Three-phase circuits with the neutral completely unbalanced (a single phase loaded) are considered a single-phase circuits.


ρ1 is the resistivity of conductors in normal service, taken equal to the resistivity at the temperature in normal service, i.e. 1,25 times the resistivity at 20 °C, or 0, 022 5 Ωmm2/m for copper and 0,036 Ωmm2/m for aluminium;


L is the straight length of the wiring systems, in metres;

 

S is the cross-sectional area of conductors, in mm2;


cos ϕ is the power factor; in the absence of precise details, the power factor is taken as equal to 0,8 (sin ϕ = 0,6);


λ is the reactance per unit length of conductors, which is taken to be 0,08 mΩ/m in the absence of other details;


IB is the design current (in amps);

 

Lebih lengkapnya bisa dilihat di standar tersebut. 

See Answer In Context

Tags (1)
4 Replies 4
HelvinHermanT
Captain Captain
Captain

Re: Berapakah maximum Drop Voltage pada instalasi listrik?

Selamat Siang juga,

 

Terima kasih atas pertanyaannya.

 

Rekomendasi maximum Drop Voltage dalam instalasi diatur dalam IEC 60364-5-52:2009 Low-voltage electrical installations – Part 5-52: Selection and erection of electrical equipment – Wiring systems

 

Bisa dilihat dalam Annex / Lampiran G mengenai "Volrtage drop in customers installations". Nilai maximum drop voltage adalah 3 - 8 % tergantung tipe instalasinya dan peruntukannya (Penerangan atau lain lain). 

 

Contoh :

Maximum drop voltage sebesar 3% untuk Penerangan (Lighting) jika disuplai dari Distribusi Listrik Umum tegangan rendah (PLN) dan maximum 6% untuk penerangan dengan suplai dari distribusi listrik tegangan rendah Privat.

Untuk penggunaan lainnya (selain penerangan) maximum drop voltage 5-8% untuk Distribusi Umum dan Private.

 

Dimungkinkan drop voltage lebih besar saat starting motor atau gawai dengan inrush current besar.

 

Voltage Drop Formula.jpg

 

Tags (1)
BudiThamrin
Crewman
Crewman
0 Likes
2
174

Re: Berapakah maximum Drop Voltage pada instalasi listrik?

Terima kasih atas informasinya, Pak @HelvinHermanT !

Untuk rumus di atas, mohon maaf ada legend lengkapnya ngga ya Pak? Seperti S, lamda, Ib, maksudnya apa, Karena terpotong.

 

Terima kasih!

Tags (1)
HelvinHermanT
Captain Captain
Captain
0 Likes
1
169

Re: Berapakah maximum Drop Voltage pada instalasi listrik?

 

u is the voltage drop in volts;
b is the coefficient equal to 1 for three-phases circuits, and equal to 2 for single-phasecircuits;


NOTE 3 Three-phase circuits with the neutral completely unbalanced (a single phase loaded) are considered a single-phase circuits.


ρ1 is the resistivity of conductors in normal service, taken equal to the resistivity at the temperature in normal service, i.e. 1,25 times the resistivity at 20 °C, or 0, 022 5 Ωmm2/m for copper and 0,036 Ωmm2/m for aluminium;


L is the straight length of the wiring systems, in metres;

 

S is the cross-sectional area of conductors, in mm2;


cos ϕ is the power factor; in the absence of precise details, the power factor is taken as equal to 0,8 (sin ϕ = 0,6);


λ is the reactance per unit length of conductors, which is taken to be 0,08 mΩ/m in the absence of other details;


IB is the design current (in amps);

 

Lebih lengkapnya bisa dilihat di standar tersebut. 

Tags (1)
BudiThamrin
Crewman
Crewman

Re: Berapakah maximum Drop Voltage pada instalasi listrik?

Siap, terima kasih informasinya Pak @HelvinHermanT !

Tags (1)