New in the Community? Get started here

Schneider Electric Exchange Community

Discuss and solve problems in energy management and automation. Join conversations and share insights on products and solutions. Co-innovate and collaborate with a global network of peers.

Register Now
Efficiency Forum
This Forum is aimed to support Power Distribution Professionals, involved in design or implementation of Power Distribution. It deals especially with Efficiency: Green & Sustainability, as well as Active Energy Management
cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 
Cadet

Reasons for MSPs to Backup Office 365

Office 365 gives its clients the recognizable advantageous interface and guarantees the security of their information regardless.

However, in spite of the fact that Office 365 ensures 100% uptime, despite everything it can’t shield you from information misfortune. The inherent Office 365 backup alternatives are very restricted and can give you AES 256-bit Encryption with Incremental backup facility.

There are Multiple ways you may lose Office 365 information. Among them are…

Malware and ransomware
File forming, prior variants can be lost
Client synchronize issues
Accidental or deliberate erasure of information
There are primary reasons why MSPs ought to give an Office 365 backup administration:

1) Files Are Deleted Due to Retention Policy

Commonly, when a man utilizes online administrations he’s certain that the information will be open at any conditions and erases pointless records decisively being certain that they can simply be recovered from junk, similarly as they were with on-premises arrangements. Be that as it may, the Office 365 waste organizer keeps its own threats.

Office 365 has its own retention arrangements for erased information. For end-clients it makes up 30 days, for administrators somewhat more, yet at the same time it’s not interminable.

If the information is erased out of this retention period, it can never be recovered again. In any case, this is the place oversaw specialist co-ops can encourage their clients.

2) Restore Deleted Emails

For each organization that speaks with the customers by means of online tools, apparatus for regular undertakings. On the off chance that a vital email is erased for all time, the organization may bear immense data loss. The mailbox has its own retention policies.

Get your server backed up using EdbMails and backup all your mailboxes automatically.

Features / Advantages of EdbMails Office 365 Email Backup With AES 256-bit encryption.

 

office-365-backup

 

AES 256-bit Encrypted, Incremental and Highly Compressed Backup
You can set Private Encryption Key for the backup for an additional protection for your data

Save Office 365 Mailbox backup on your local computer or on network / shared drives
Incremental backup: Consecutive backup will only backup newly added items to your mailbox there by saves bandwidth, disk space and time.
Keeps up to 30 incremental versions on your local backup
Highly Compressed and Incremental backup will enhance backup performance
Granular backup of Office 365 mailbox can backup Emails, Contacts, and Calendar, task etc.
Configure backup in 2 clicks by using ease of use and user-friendly application interface.
Filter Office 365 Mailbox backup by Date, Subject, Attachment, Email address etc.
Backup single mailbox as well as multiple mailboxes from Office 365
Backup office 365 mailbox to pst
Backup Archive Office 365 mailboxes
Backup Public folder Office 365 mailbox

 

 

More info: Office 365 backup mailbox