Invite a Co-worker
Send a co-worker an invite to the Exchange portal.Just enter their email address and we’ll connect them to register. After joining, they will belong to the same company.
Send Invite Cancel
79399members
344145posts

Ecostruxure Power Design MTZ circuit breaker thermal settings

pascal44210
Cadet
0 Likes
1
219

Ecostruxure Power Design MTZ circuit breaker thermal settings

Hi,

I've just downloaded and installed new INT 4.9.7 & FR 4.9.4 releases of Ecostruxure Power Design and the MTZ breaker thermal setting facility is not updated yet.

 

Indeed, with actual micrologic tripping units, thermal settings are adjustable amp by amp like NSX MCCB (5.2 or 5.3).

 

Currently, in Power Design, only fixed values are available replicated from old NT/NW trip units.

 

Could you update quickly the soft to take account the good set facility with a patch or a sub release ?

 

Thank you in advance

 

 

Tags (1)
1 Reply 1
Genghiz
Lieutenant Lieutenant
Lieutenant
0 Likes
0
183

Re: Ecostruxure Power Design MTZ circuit breaker thermal settings

Hello,

 

Thanks for this inputs. 

 

This fine settings of the latest trip units are already informed as a requirement.

 

This is listed as part of product backlog, and also the implementaion feasibility is under analysis now.

 

Based on the conclusion of the analysis this will be considered for implementation.

 

Regards, 

Ecodial Expert Support.

Tags (1)