EcoStruxure Power Design Forum
Schneider Electric support forum to share knowledge about installation and usage for Electrical Network Design and Calculation Software (Ecodial, Ecostruxure Power Design).
Link copied. Please paste this link to share this article on your social media post.
Posted: 2021-02-15 09:42 PM . Last Modified: 2021-02-21 03:46 PM
Following are the offers integrated and made available at the "EcoStruxure Power Design - Ecodial INT 4.9.5" version of the application.
Other Offers :
Easy series Offer integration
CIRCUIT BREAKER - EasyPact™ CVS Breaker:
CIRCUIT BREAKER- EasyPact™ MVS Breaker:
CIRCUIT BREAKER - EasyPact™ EZC:
SWITCHES:
Link copied. Please paste this link to share this article on your social media post.
Link copied. Please paste this link to share this article on your social media post.
Posted: 2021-02-16 01:46 AM
@Genghiz hello
For which countries is this version available?
Where can I download EcoStruxure Power Design - Ecodial INT 4.9.5?
Thanks in advance
Link copied. Please paste this link to share this article on your social media post.
Link copied. Please paste this link to share this article on your social media post.
Posted: 2021-02-16 01:50 AM
This is the international version and applicable where IEC standards are followed. You can download the software here
Regards,
Arjun
Link copied. Please paste this link to share this article on your social media post.
Link copied. Please paste this link to share this article on your social media post.
Posted: 2021-02-16 01:56 AM
Link copied. Please paste this link to share this article on your social media post.
Link copied. Please paste this link to share this article on your social media post.
Posted: 2021-06-09 06:59 AM
what about use of single core cables 630 to 1000 sq.mm in ECODIAL for Transformer LV side to Main LV panel which is a prevalent practice in middle east? Currently this feature is not available. Lack of this feature is giving wrong results to us engineers in Gulf. How about adding this feature?
Link copied. Please paste this link to share this article on your social media post.
Link copied. Please paste this link to share this article on your social media post.
Posted: 2021-06-09 10:34 PM
Hi @dkpElect
Thanks for your query.
In the latest International V4.9.5 version. This feature is already added. Now the user will be able to select the required cable cross-sectional area up to 1000sq.mm and Ecodial will be able to size the optimum cable CSA.
Here I attached the screenshot of your reference.
In this example, I have selected 1000sq.mm as the max permissible CSA. The application is proposing the best-suited cable CSA based on the transformer power.
You can download the latest International version by using this link. EcoStruxure Power Design - Ecodial
Link copied. Please paste this link to share this article on your social media post.
Link copied. Please paste this link to share this article on your social media post.
Posted: 2021-06-26 05:20 AM
Noted. Thanks for the update.
However, it is noticed that, for 3x1000 sq.mm as per phase conductor , the PE conductor also is sized as 1000 Sq.mm ( for both TT and TN-S system) whereas standard maximum size normally used is 300 sq.mm. Whether we adopt 50% of phase conductor rule or adiabatic equation, I don't think 1000 sq.mm would be required.
I checked with another similar software from SIEMENS and the result is 300 sq.mm for PE.(see image attached).
Any clarification would be highly appreciated .
Best Regards,
Dinesh
Link copied. Please paste this link to share this article on your social media post.
Create your free account or log in to subscribe to the forum - and gain access to more than 10,000+ support articles along with insights from experts and peers.