This question was originally posted on DCIM Support by Olle Forsblom on 2019-10-16
I have installed the modular PDU and connected it to DCE successfully. When the device appears in DCO it says that it matches a different modular PDU than the one I am using and I can not associate it to the correct modular PDU.
How can I solve this issue?
(CID:149785677)
Solved! Go to Solution.
This answer was originally posted on DCIM Support by Valentin Kozlov on 2019-10-17
Hi!
I believe that it's because PDU have "Modular PDU" model on your screen shot.
I suppose that serial numbers in DCO model was not configured.
DCO need Model-Name-Serial Number matching to automatic association.
Now you can associate devices manually: select PDU on the floor plan, then right-click on uassociated device at the left pan and select "Associate"
(CID:149785945)
This comment was originally posted on DCIM Support by Greg Sterling on 2019-10-16
Hello Olle
Can you share some screenshots of the device as it appears in DCO and the device its matching too? On the DCO side can you provide a screenshot of the device details as they are reported by DCE?
When DCO matches an external device to an item in DCO it will compare the item make and model, then device specific information like the device name, serial number, bar code, IP address and so on. The make and model will match against items in your local genome library.
Are there similarities in any of the above items to the item its actually matching to?
Regards
Greg Sterling
(CID:149785684)
This comment was originally posted on DCIM Support by Olle Forsblom on 2019-10-16
The issue is that it should not be matching the 100kVA Modular PDU that is 600mm wide. It should match the 277kVA Modular Remote Power Panel that is 300mm wide which is already in my genome and on my floorplan.
(CID:149785965)
This answer was originally posted on DCIM Support by Valentin Kozlov on 2019-10-17
Hi!
I believe that it's because PDU have "Modular PDU" model on your screen shot.
I suppose that serial numbers in DCO model was not configured.
DCO need Model-Name-Serial Number matching to automatic association.
Now you can associate devices manually: select PDU on the floor plan, then right-click on uassociated device at the left pan and select "Associate"
(CID:149785945)
This comment was originally posted on DCIM Support by Olle Forsblom on 2019-10-17
Thanks, it worked fine!
Regards,
Olle
(CID:149785950)
This question is closed for comments. You're welcome to start a new topic if you have further comments on this issue.
Discuss challenges in energy and automation with 30,000+ experts and peers.
Find answers in 10,000+ support articles to help solve your product and business challenges.
Find peer based solutions to your questions. Provide answers for fellow community members!