Dears,
In the project which is a running data center the customer needed from us to communicate with STULZ Cooling units via Modbus protocol to be added in the DCE server through EGX150.
but after adding the devices to the DCE server, we used attached ddf as we expected that it will work. but it give us only the communication status of the device and there are no further readings or measurements. So please advise.
Regards,
Magdy
Hi Magdy,
What is the model number of the cooling unit you are trying to connect? And if you have the Modbus map for it, can you attach or link it?
Thanks,
Jake
Discuss challenges in energy and automation with 30,000+ experts and peers.
Find answers in 10,000+ support articles to help solve your product and business challenges.
Find peer based solutions to your questions. Provide answers for fellow community members!