This question was originally posted on DCIM Support by Pavel Andreev on 2019-09-30
Could you please clarify for me question of out-of-box integration of DCO and SCOM 2016 R2. Based on information from manual - it's impossible. Is it right?
Pavel
(CID:149292853)
This answer was originally posted on DCIM Support by Jef Faridi on 2019-09-30
Hi Pavel,
If you are referring to integrating with Virtual Machine Manager through StruxureWare Data Center Operation: PRO Pack (https://sxwhelpcenter.ecostruxureit.com/display/UADCO8x/StruxureWare+Data+Center+Operation%3A+PRO+Pa...) , then yes, that should be possible in DCO 8.x.
Kind regards
(CID:149292864)
This comment was originally posted on DCIM Support by Pavel Andreev on 2019-09-30
Thank you Jef. I see possibility of SCOM integration, but my question is about exact SCOM 2016 R2 version.
(CID:149292989)
This comment was originally posted on DCIM Support by Jef Faridi on 2019-10-01
Hi Pavel,
We haven't tested that, so I cannot offer a clear answer about the exact version. Do you see issue with integration? If the integration/communication is through http, then make sure the "Redirect HTTP to HTTPS" is not enabled in DCO.
Kind regards
(CID:149292991)
This comment was originally posted on DCIM Support by Pavel Andreev on 2019-10-01
Thank you, Jef.
I'll try.
Pavel
(CID:149293029)
This question is closed for comments. You're welcome to start a new topic if you have further comments on this issue.
Discuss challenges in energy and automation with 30,000+ experts and peers.
Find answers in 10,000+ support articles to help solve your product and business challenges.
Find peer based solutions to your questions. Provide answers for fellow community members!