This question was originally posted on DCIM Support by Yaniv Rozenbaum on 2019-10-07
Hi,
I'm having an issue while trying to install a DCO version 8.2.12 on a REDHAT system I see notifications for DB installation attachments failure Picture of the messages
All the required steps in the document:
https://sxwhelpcenter.ecostruxureit.com/display/public/UADCO8x/Installing+DCO+on+Red+Hat+Enterprise+...
The installation on this server was done precisely as in the document
I wanted to know if DCO version 8.2.12 has been tested for installation on REDHAT and whether any prerequisites or installations are required on the server before installing the DCO software on the server?
the server do not have internet connection!!
regards ,
Yaniv Rozenbaum
(CID:149783164)
This answer was originally posted on DCIM Support by Jef Faridi on 2019-10-17
Hi Yaniv,
I have recently tested DCO 8.2.12 and 8.3.x installation on a Redhat sever with Internet access, that did not work. It seems this installation feature may need to be investigated/updated - I logged an enhancement report for this.
Kind regards
(CID:149785992)
This comment was originally posted on DCIM Support by Dalibor Barucak on 2019-10-21
Hello Jef,
our customer deals with the same problem. DCO 8.3.2 installation on RHEL 7.6. After a few tries, they find a problem with the installation script (looks like there is an unexpected yum request to a user).
DCO server is running now, but it looks like they're still some issues linked with that. So I would be grateful if this feature will be check.
Kind regards,
Dalibor Barucak
(CID:149786767)
This question is closed for comments. You're welcome to start a new topic if you have further comments on this issue.
Discuss challenges in energy and automation with 30,000+ experts and peers.
Find answers in 10,000+ support articles to help solve your product and business challenges.
Find peer based solutions to your questions. Provide answers for fellow community members!