Invite a Co-worker
Send a co-worker an invite to the Exchange portal.Just enter their email address and we’ll connect them to register. After joining, they will belong to the same company.
Send Invite Cancel
80679members
346672posts

Network Cabling Issue

Solved
barlasbaycik1
Ensign
Ensign
0 Likes
1
179

Network Cabling Issue

Hello,

 

I need to connect cables between floors. But We created all flats as a New Server Room. So I need to connect network cables between two server rooms. How can we do this. ı couldn't see the other server room when ı connect cables.

 

Best Regards;

Barlas

Tags (1)

Accepted Solutions
Jef
Captain Captain
Captain

Re: Network Cabling Issue

Hi Barlas,

 

To make a network connection between two patch panels located in two different rooms, try as illustrated:

In patch panels properties > Network, select a configured port (1) , click Connect to... (2) , select room (3) and continue the configuration.

 

Capture_jf1.JPG

 

Kind regards,

Jef

 

See Answer In Context

Tags (1)
1 Reply 1
Jef
Captain Captain
Captain

Re: Network Cabling Issue

Hi Barlas,

 

To make a network connection between two patch panels located in two different rooms, try as illustrated:

In patch panels properties > Network, select a configured port (1) , click Connect to... (2) , select room (3) and continue the configuration.

 

Capture_jf1.JPG

 

Kind regards,

Jef

 

Tags (1)