This question was originally posted on DCIM Support by Kevin Kolobe on 2020-01-31
Hi,
I have a Netbotz 750 running firmware 5.2.0. I have 2 x leak ropes and 6 x dry contacts on board with 5 x sensor pods on the A-link bus.
All my sensors are showing disconnected although all sensor pods are on and recording. Any suggestions what the issue could be?
Note that i have a power supply on the one of the sensor pods and have added an additional power supply for testing which has not help one bit.
Kevin
(CID:154796102)
This comment was originally posted on DCIM Support by GavOB on 2020-01-31
Hi Kevin Kolobe,
Had they been working or is this a new install?
What model are the sensor pods, do you have any sensors connected directly and if so are they showing up as disconnected too?
-Gavan
(CID:154796132)
This comment was originally posted on DCIM Support by Kevin Kolobe on 2020-01-31
Hi Gavan,
The solution had been running fine and has been deployed for about 2 months now.
All sensor pods are NBPD0155s. 2 of pods have 2 x spot fluids and a door sensor and the rest are only monitoring the room temperature and humidity. On the appliance itself we have 6 x dry contacts and are using both the leak rope ports.
Kevin
(CID:154796176)
This question is closed for comments. You're welcome to start a new topic if you have further comments on this issue.
Discuss challenges in energy and automation with 30,000+ experts and peers.
Find answers in 10,000+ support articles to help solve your product and business challenges.
Find peer based solutions to your questions. Provide answers for fellow community members!