Invite a Co-worker
Send a co-worker an invite to the Exchange portal.Just enter their email address and we’ll connect them to register. After joining, they will belong to the same company.
Send Invite Cancel
80607members
346537posts

Netbotz 750 firmware 5.2.1 and no comunication from vlan

RCastillo
Crewman
Crewman

Netbotz 750 firmware 5.2.1 and no comunication from vlan

A client with a netbotz 750 and firmware 5.2.1 has access from same vlan to netbotz. When they are connected in another vlan, they are unable to see the netbotz. They say that the issue is oddly in this device only and no other have problems. I have asked them to upgrade firmware, but meanwhile have you heard about something similar?? 

Tags (1)
1 Reply 1
masolans
Ensign
Ensign
0 Likes
0
162

Re: Netbotz 750 firmware 5.2.1 and no comunication from vlan

I have same problem

Tags (1)