Hello Everyone
I have a NetBotz 455 running on v4.7 that I wish to Configure SMS Alerts. However when I connect the GSM Modem via the USB Port, the NetBotz is not showing that a Serial Device has been connected via the USB Port.
I configreset the NetBotz, changed the Firmware to lower versions but still the GSM is not being displayed on the NetBotz.
I have used the same type of GSM Modem on other NetBotz 455s and it works perfectly fine.
Anyone with a solution to this problem?
Thank you in advance.
Hi @Mr_T
Have you tried searching the APC FAQs? This article discusses supported modems:
https://www.apc.com/us/en/faqs/FA158359/
I'd suggest contacting support if you haven't solved the issue by now.
Best,
Jackie
Discuss challenges in energy and automation with 30,000+ experts and peers.
Find answers in 10,000+ support articles to help solve your product and business challenges.
Find peer based solutions to your questions. Provide answers for fellow community members!