Wondering if the lithium Smart-UPS products are fully compatible with DCE?
If so, do they need to have management cards installed or can the built-in SmartConnect port be used for this?
Hi,
The Lithium SmartUPS should be fully compatible when used with an appropriate network card (AP9640/41, legacy 30/31/35), but unfortunately the smartconnect ports are single-purpose.
Discuss challenges in energy and automation with 30,000+ experts and peers.
Find answers in 10,000+ support articles to help solve your product and business challenges.
Find peer based solutions to your questions. Provide answers for fellow community members!