41333members
184398posts

Latest DCO Catalogue

Highlighted

Latest DCO Catalogue

Hi i had a request for a device to be added into DCO before the forum changed, how do i find out if its been addressed and where can i get the latest genome update for DCO

TIA

Mike

1 REPLY 1
Highlighted
Lieutenant JG Lieutenant JG
Lieutenant JG

Re: Latest DCO Catalogue

Hi Mike,

 

The latest genome updates are from Nov. 2019, so perhaps it might include some, But this is something you can verify/test your self,

check Genome Library update (in your setup), desktop client, Properties > Genome Library

If it should say something like 11/8/19, then you have the latest update.

Capture.JPG

 

Then look in your Genome Library and see if your device(s) is/are included.

 

I think the new genome update is expected in the next few months.

 

If you don't have the latest genome update (from Nov. 2019) which is compatible with DCO 8.3.2 (and ITA 9.0.x), then for the time being you might want to post a request per email: support@ecostruxureit.com

 

Kind regards