Invite a Co-worker
Send a co-worker an invite to the Exchange portal.Just enter their email address and we’ll connect them to register. After joining, they will belong to the same company.
Send Invite Cancel
80810members
346874posts

Isusue with 4K ITA client

Solved
TonKei
Lieutenant JG Lieutenant JG
Lieutenant JG
0 Likes
1
1221

Isusue with 4K ITA client

Hi Team

 

My customer is using a 4K display and when the resolution is set to 4K, the labels in the rack is enlarged compared to using the client at a smaller resolution. Please see attached screenshots.

 

Best regards

Tonny Keinicke 

Attachments

Accepted Solutions
Jef
Captain Captain
Captain

Re: Isusue with 4K ITA client

Hi Tonny,

 

Which browser are you using? please try with Chrome, if haven't done that already. 

We have recently experienced that the web-client may have unexpected behavior on high resolution screen setup. This has been captured in our backlog for investigation. In the mean time I would go for lowering the screen resolution and/or lower the displayed browser window.

 

Kind regards

 

---

update:

 

I've just noticed (from your screen shoots) that you are seeing the issue on desktop client, wondering if the following change could help a little. Assuming the Display size is set to 100%. Right click on the application/EcoStruxure IT Advisor shortcut (on your windows desktop) Properties > Compatibility > Change high DPI settings > and then click/enable "Override high DPI scaling behavior. Scaling performed by: select "System" from the list. and OK, 

Capture-1.JPG

 

See Answer In Context

1 Reply 1
Jef
Captain Captain
Captain

Re: Isusue with 4K ITA client

Hi Tonny,

 

Which browser are you using? please try with Chrome, if haven't done that already. 

We have recently experienced that the web-client may have unexpected behavior on high resolution screen setup. This has been captured in our backlog for investigation. In the mean time I would go for lowering the screen resolution and/or lower the displayed browser window.

 

Kind regards

 

---

update:

 

I've just noticed (from your screen shoots) that you are seeing the issue on desktop client, wondering if the following change could help a little. Assuming the Display size is set to 100%. Right click on the application/EcoStruxure IT Advisor shortcut (on your windows desktop) Properties > Compatibility > Change high DPI settings > and then click/enable "Override high DPI scaling behavior. Scaling performed by: select "System" from the list. and OK, 

Capture-1.JPG