Invite a Co-worker
Send a co-worker an invite to the Exchange portal.Just enter their email address and we’ll connect them to register. After joining, they will belong to the same company.
Send Invite Cancel
80675members
346659posts

IT Advisor 9.2.3 released

JLehr
Lt. Commander Lt. Commander
Lt. Commander
0 Likes
0
1132

IT Advisor 9.2.3 released

In this release:

  • You can now model cable trays in 2D in the IT Advisor desktop client. This feature will be built upon to include modeling network cable routing and calculating cable length later this year. 
  • Asset UIDs are now visible in the desktop client. More...
  • The genome packages added with the last 3 releases of ITA are now bundled in ITA 9.2.3.
  • Bug fixes
  • Security fxes

See What's new in IT Advisor 9.2.x

 

Known issue

Some users have reported that the desktop client freezes after updating to 9.2.3.
This issue is being investigated.

Tags (1)