This question was originally posted on DCIM Support by lorenzo ferigo on 2019-11-19
i do the following with postman:
POST https://myserver/api/v8.1/authentication
Headers: "Accept" "application/json"
"Content-Type" "application/json"
Then in postman i set "No Auth" because otherwise user and password are not sent as body of the post as per documentation
Body of the request is the user and password the same way they are sent in the restapi documentation with "try it"
I always get "invalid token" in the reply but as per the documentation this is the method to be used the first time to obtain the token.
Postman is also creating the curl code corresponding to the call :
curl -X POST \
https://10.206.203.2/api/v8.1/authentication \
-H 'Accept: application/json' \
-H 'Content-Type: application/json' \
-H 'Postman-Token: b427d487-89c5-4c5e-a3cc-d940b603a8a8' \
-H 'cache-control: no-cache' \
-d '{"password": "xxxx","username": "xxxx"}'
What am i doing wrong?
Is there any ready example in python to obtain the authentication token and in general to perform some requests?
Thanks a lot fo rthe kind reply
(CID:152076809)
This answer was originally posted on DCIM Support by lorenzo ferigo on 2019-11-19
Hello , i solved the problem about authentication in postman.
But it would be nice to collect some restapi usage examples in java/python.....
(CID:152076864)
This question is closed for comments. You're welcome to start a new topic if you have further comments on this issue.
Discuss challenges in energy and automation with 30,000+ experts and peers.
Find answers in 10,000+ support articles to help solve your product and business challenges.
Find peer based solutions to your questions. Provide answers for fellow community members!