This question was originally posted on DCIM Support by Wes Burhoe on 2019-11-05
Specifically, In the case where a circuit previously had load... which was manually imported at some point in the past, but now I am manually importing a 0 load on the given poles. This use case is where there used to be a circuit, but has since been removed so I need to reset the measurements to the proper load. The same use case applied when loads in generally are going down... where we know DCO is maintaining historical peak readings.
(CID:151062965)
This answer was originally posted on DCIM Support by Jef Faridi on 2019-11-06
Hi Wes,
I think usually the measured data should be updated after 30 days period, otherwise it may need to be investigated. Our team will be investigating this as soon as possible (we are aware of your issue with some devices not changing to 0 load).
Kind regards
(CID:151063212)
This question is closed for comments. You're welcome to start a new topic if you have further comments on this issue.
Discuss challenges in energy and automation with 30,000+ experts and peers.
Find answers in 10,000+ support articles to help solve your product and business challenges.
Find peer based solutions to your questions. Provide answers for fellow community members!