Invite a Co-worker
Send a co-worker an invite to the Exchange portal.Just enter their email address and we’ll connect them to register. After joining, they will belong to the same company.
Send Invite Cancel
80616members
346561posts

EcoStruxure IT Advisor 9.1.4 released

JLehr
Lt. Commander Lt. Commander
Lt. Commander
0 Likes
5
1383

EcoStruxure IT Advisor 9.1.4 released

The IT Advisor 9.1.4 release contains the following fixes:

 

  • The Table view in Web Client now includes the customer filter option.
  • The Table view now sorts as expected when the customer column is enabled.
  • Exporting in Table view now works as expected when the customer column is enabled.

 

You can find the ITA release notes, recent changes, improvements, and more in the EcoStruxure IT Help Center.

Tags (1)
5 Replies 5
Jerome_C
Ensign
Ensign
0 Likes
1
1282

Re: EcoStruxure IT Advisor 9.1.4 released

Thank you for this news,

 

Where can i get the download link of this new release ?

Can i upgrade from 9.1.0  or i need a clean installation with a backup to upgrade to this last release ?

 

Kind regards,

Tags (1)
gsterling
Commander Commander
Commander
0 Likes
0
1274

Re: EcoStruxure IT Advisor 9.1.4 released

Hello Jerome.

 

You can browse to https://ecostruxureit.com/  and click the "submit a ticket" button or email support@ecostruxureit.com to request the ITA 9.1.4 download links.

 

It is helpful if you provide your support contract id so the team can validate an active support contract.

 

In regards to the update, if you are already running ITA 9.1.0 or newer, you can directly upgrade to ITA 9.1.4 using webmin and the checksum file for the iso image provided on the download page. The upgrading section of this page describes the process of using webmin to upgrade your installation.

https://helpcenter.ecostruxureit.com/hc/en-us/articles/360009560538-Upgrading-from-DCO-8-x-to-IT-Adv...

 

Regards

 

Greg Sterling

Tags (1)
bklotzodu
Crewman
Crewman
0 Likes
2
1158

Re: EcoStruxure IT Advisor 9.1.4 released

Hi Folks,

  We need a silent install switch to be able to install this application for our users via InTune.  When will that feature be added to your installers?

Tags (1)
cyrielle-b
Crewman Crewman
Crewman
0 Likes
1
1138

Re: EcoStruxure IT Advisor 9.1.4 released

Hi Brian,

 

Thanks for the feedback.

 

This function isn't currently on our roadmap, however I have documented it in our backlog for us to take a look at and possibly prioritize.

 

Best,

 

Cyrielle

Tags (1)
bklotzodu
Crewman
Crewman
0
1134

Re: EcoStruxure IT Advisor 9.1.4 releasThanked

Thanks, Cyrielle.  Like others in the IT industry, we are trying to "Do More with Less" and thus reducing our support overhead costs.  Not having to engage our IT Support to install the software or having it necessary for our users to have admin rights to install it is a significant benefit, especially with so many of our users and technicians working remotely.

Tags (1)