43299members
217682posts

Does NBES0201 still is supported by netbotz?

Highlighted

Does NBES0201 still is supported by netbotz?

This question was originally posted on DCIM Support by Victor Juarez Velazquez on 2020-01-24


Does NBES0201 (APC NetBotz Particle Sensor PS100) still is supported by some netbotz appliance or sensor pod?

According  to installation manual, it needs a 6 Pin port, and as afar as i know there is no such port available on any current sensor port.

https://download.schneider-electric.com/files?p_File_Name=ASTE-6Z5S83_R0_EN.pdf&p_Doc_Ref=SPD_ASTE-6...

 

 

 

(CID:154403198)

3 REPLIES 3
Highlighted

Re: Does NBES0201 still is supported by netbotz?

This answer was originally posted on DCIM Support by Cory McDonald on 2020-01-24


Victor Juarez Velazquez,

There is no solution that can be sold for the NBES0201 particle sensor.  It required a V2 appliance or a Sensor Pod 120, both of which are end-of-sale and end-of-support.  There is no current NetBotz Solution that can be sold for a particle sensor.

You may be able to find a third party sensor that can communicate via: 4-20mA, 0-5V, or dry contacts; but I have not looked into a possible integration that way.

Regards,

Cory

(CID:154403201)

Highlighted

Re: Does NBES0201 still is supported by netbotz?

This answer was originally posted on DCIM Support by Victor Juarez Velazquez on 2020-01-24


So clear

(CID:154403508)

Highlighted

🔒 Closed

This question is closed for comments. You're welcome to start a new topic if you have further comments on this issue.