This question was originally posted on DCIM Support by Gianluca Bertuletti on 2018-10-24
Hi All
someone can explain how does it work "You can now change the IP addresses of discovered nodes without losing data"
thanks
(CID:134688419)
Solved! Go to Solution.
This answer was originally posted on DCIM Support by Law TJ on 2018-10-24
Hi,
Previous version OF DCE, when your device changes ip, you will need to rediscover the device and add into DCE. This 'existing device' will be seen as new device in DCE and you will lost the device data, if you delete the device with its old IP.
For new DCE, you can change your device IP under device settings and the data logging will continue with the new IP.
Hope this helps.
(CID:134688524)
This answer was originally posted on DCIM Support by Law TJ on 2018-10-24
Hi,
Previous version OF DCE, when your device changes ip, you will need to rediscover the device and add into DCE. This 'existing device' will be seen as new device in DCE and you will lost the device data, if you delete the device with its old IP.
For new DCE, you can change your device IP under device settings and the data logging will continue with the new IP.
Hope this helps.
(CID:134688524)
This comment was originally posted on DCIM Support by Stephen Wellings on 2018-10-24
When did that become an option? In 7.6.0?
(CID:134688610)
This comment was originally posted on DCIM Support by Gianluca Bertuletti on 2018-10-24
Hi
if im going to change ip address of a device, i have to discover the new ip and delete the other one. is that correct?
the only thing that remains is history with new Dce.
but i have to re-create all the threshold
(CID:134688634)
This comment was originally posted on DCIM Support by Steven Marchetti on 2018-10-24
Hi Gianluca,
No, you do not re-discover the device. As Law TJ mentioned, you simply need to change your device IP under device settings. If you delete the device and re-add it or re-add it under the new IP, you will either lose the old data or not be able to sync the old and new data, you'd have 2 devices.
You simply go to the device scan settings and replace the old IP with the new IP:
Each device must be done individually in this dialog box.
Stephen Wellings, yes it is new to 7.6.
Thanks,
Steve
(CID:134688677)
This comment was originally posted on DCIM Support by Law TJ on 2018-10-24
Thanks Steve for the detailed answer.
(CID:134688709)
This comment was originally posted on DCIM Support by Christopherus Laurentius on 2018-10-25
+1 on this very useful feature.
A short video or GIF of that would be great....😉
(CID:134689094)
This question is closed for comments. You're welcome to start a new topic if you have further comments on this issue.
Discuss challenges in energy and automation with 30,000+ experts and peers.
Find answers in 10,000+ support articles to help solve your product and business challenges.
Find peer based solutions to your questions. Provide answers for fellow community members!