43296members
217681posts

Data Center Expert - Export email in Graph format

Highlighted
Crewman

Data Center Expert - Export email in Graph format

I'm running DCE 7.8.0 and have an APC PDU 8841 with an APC Temp sensor connected. I would like to get a daily email in graph format of the temps for the last 24hrs. Can this be done?

 

I can get the report in csv but cant figure out a way in graph format, Suggestions?

 

Thank You

Tags (1)
3 REPLIES 3
Highlighted
Lieutenant JG

Re: Data Center Expert - Export email in Graph format

Hi @kstory ,

 

At present, this isn't an option. The best way is to export the data and bring it into Microsoft Excel or some other tool that can do graphing. This is a known issue ans has been entered as an enhancement request. I've added this port to that enhancement request as the more people that request this type of thing, the more likely it will get addressed. There is no current timeframe as to when this might be added to the system, Sorry.

 

Thanks,

Steve

Tags (1)
Highlighted
Crewman

Re: Data Center Expert - Export email in Graph format

Thank you for the information

 

Do you know of anyway i can accomplish this with the APC PDU?

Tags (1)
Highlighted
Lieutenant JG

Re: Data Center Expert - Export email in Graph format

Hi @kstory 

 

The graphing, reporting, and exporting functionality of DCE is device independent. 

 

The PDU on it's own, although it has a graphing feature, does not have an automated export functionality.

 

Steve

Tags (1)