This question was originally posted on DCIM Support by Lukasz Staciwo on 2019-03-11
Hi Team,
Asking on behalf of the customer Jimmy Leung.
In the current version of DCO a CRAC unit monitored by DCE will show the Temprerature and Humidity sensors that can subsequently be positioned on the floor in the DCO layout.
Are there any plans in bringing across other sensors like fan speed and cooling output figures so DCO can use those and adjust the cooling calculations?
(CID:140712543)
Solved! Go to Solution.
This answer was originally posted on DCIM Support by Jef Faridi on 2019-03-11
Hi Lukasz,
For the time being there are no plans to change the DCE sensor mapping functionality to DCO (https://sxwhelpcenter.ecostruxureit.com/display/DCIMDEVELOPER/DCE+Sensor+Mapping+to+DCO). However, the near future plan is to add more functionality into the webclient.
Kind regards
(CID:140712639)
This answer was originally posted on DCIM Support by Jef Faridi on 2019-03-11
Hi Lukasz,
For the time being there are no plans to change the DCE sensor mapping functionality to DCO (https://sxwhelpcenter.ecostruxureit.com/display/DCIMDEVELOPER/DCE+Sensor+Mapping+to+DCO). However, the near future plan is to add more functionality into the webclient.
Kind regards
(CID:140712639)
This comment was originally posted on DCIM Support by Lukasz Staciwo on 2019-03-12
Thanks Jeff,
Could you kindly log it as a Feature Request.
I will send end user details over direct email.
(CID:140712922)
This question is closed for comments. You're welcome to start a new topic if you have further comments on this issue.
Discuss challenges in energy and automation with 30,000+ experts and peers.
Find answers in 10,000+ support articles to help solve your product and business challenges.
Find peer based solutions to your questions. Provide answers for fellow community members!