This question was originally posted on DCIM Support by Yannick BARRAUD on 2019-05-15
Hi
The upgrade failed with many package errors
see upgrade log: 20190515 DCO Dev Upgrade 8.3 - Tentative 1.txt
Please note that I set the option "Do not download packages from the Internet"
Any ideas?
Best Regards
Yannick
(CID:143758351)
This answer was originally posted on DCIM Support by Jef Faridi on 2019-05-15
Hi Yannick,
Wondering if you had also checked the option that says "No thirdparty RPMs" ?
if the answer is yes, then please try only with checking the option "Do not download packages from the Internet".
Thanks,
Kind regards
(CID:143758363)
This comment was originally posted on DCIM Support by Yannick BARRAUD on 2019-05-15
Hi Jef
No I had not
I also tried with this option in addition of "Do not download packages from the Internet".
The upgrade succeeded (see log in attachment) but I know this upgrade path is not recommended as nobody in our environment manage the thirdparty packages for the moment
20190515 DCO Dev Upgrade 8.3 - Tentative 3.txt
Kind Regards,
Yannick
(CID:143758500)
This comment was originally posted on DCIM Support by Jef Faridi on 2019-05-15
Hi Yannick,
Many thanks for the update. Glad to hear the latest upgrade attempt was successful, thanks.
Kind regards
(CID:143758503)
This comment was originally posted on DCIM Support by Yannick BARRAUD on 2019-05-15
Successful sure but I am not fully satisfied as the thirdparty RPMs have not been updated
(CID:143758505)
This comment was originally posted on DCIM Support by Jef Faridi on 2019-05-15
Hi Yannick,
If the upgrade process successfully upgrades to 8.3, then all should be good. The option for third party files usually may be relevant for custom installations on Redhat server.
By the way, it is important to not interrupt the upgrade processes (by leaving the upgrade page or manually restarting the server).
Kind regards
(CID:143758516)
This answer was originally posted on DCIM Support by Andrew Stoakes on 2019-05-16
Had the same issue last night when upgrading to v8.3. I had to select both "Do not download packages from the Internet" and "No third party RPMs" for the upgrade to be successful.
Seams to be working fine.
(CID:143758774)
This question is closed for comments. You're welcome to start a new topic if you have further comments on this issue.
Discuss challenges in energy and automation with 30,000+ experts and peers.
Find answers in 10,000+ support articles to help solve your product and business challenges.
Find peer based solutions to your questions. Provide answers for fellow community members!