This question was originally posted on DCIM Support by Ahmed Ashraf on 2019-08-28
Dears,
While adding the network routing (ports connection) from switches ports to patch panels ports & field equipment (UPS, NetBotz, CRAH units, Servers).
The network utilization percentage displayed on the pie chart considered only the ports connected to field equipment and neglected patch panels connections (considered them not-utilized ports).
Then, How to overcome this issue? How to consider all switches ports connection (even connected to field device or patch panel) in network utilization percentage?
Note: The patch panels rear side connected to other systems devices (Cameras, Control panels, Chillers , ... etc.).
Regards,
Ahmed Ashraf
(CID:148343654)
This answer was originally posted on DCIM Support by Jef Faridi on 2019-08-28
Hi Ahmed,
Patch panels (similar to cables) are not included in the Capacity Overview calculations. Network ports in layer 2 & 3 network equipment (such as server/switch) are included in the capacity history KPIs.
Kind regards
(CID:148343663)
This comment was originally posted on DCIM Support by Ahmed Ashraf on 2019-08-28
Dear Greg,
I understand what you say, But there is no cameras (as example) in DCO
Then how to utilize all switches ports of cameras to be considered in Network utilization calculations.
Regards,
Ahmed
(CID:148344011)
This comment was originally posted on DCIM Support by Jef Faridi on 2019-08-29
Hi Ahmed,
As a work around I would try customizing/using a switch device and call it "camera switch" and then configure its network ports and set its power settings to zero, without power inlets (to not include in power capacity calculations).
Kind regards
(CID:148344014)
This comment was originally posted on DCIM Support by Ahmed Ashraf on 2019-08-29
Dear Jef,
OK, i did this work around and i'll check the network utilization update tomorrow and back to you with updates
Thanks for your support
Regards,
Ahmed Ashraf
(CID:148344097)
This question is closed for comments. You're welcome to start a new topic if you have further comments on this issue.
Discuss challenges in energy and automation with 30,000+ experts and peers.
Find answers in 10,000+ support articles to help solve your product and business challenges.
Find peer based solutions to your questions. Provide answers for fellow community members!