This question was originally posted on DCIM Support by Yannick BARRAUD on 2017-03-13
With DCO 8.0.4 (perhaps 8.0.3) we can no longer set in a rack PDU power dependency tab a power supply which is not located in the same room.
Is it a normal behaviour or a bug?
Fortunately we can set the power path from the supplies to the PDUs
(CID:113644682)
This answer was originally posted on DCIM Support by Jef Faridi on 2017-03-13
Hi Jannick,
You are right, currently it is not possible to connect a rack pdu to power supply that is located in another room - but as you have mentioned it can be configured from the power distribution unit (PDU) itself. We have recently registered an enhancement case for this, thanks.
Kind regards
(CID:113644696)
This question is closed for comments. You're welcome to start a new topic if you have further comments on this issue.
Discuss challenges in energy and automation with 30,000+ experts and peers.
Find answers in 10,000+ support articles to help solve your product and business challenges.
Find peer based solutions to your questions. Provide answers for fellow community members!