This question was originally posted on DCIM Support by Mate Fekete on 2019-08-13
I have problem with DCE - Synchronized backup because it's getting failure. I'm using NFS share to store the backup. On the same NFS the Full and Configuration type of backups are running error free:
What am I doing wrong? Previously sync backup worked fine but about 2 weeks before something happened.
DCE version is 7.6.0 and server uptime is 6 days.
(CID:147783942)
This answer was originally posted on DCIM Support by Mate Fekete on 2019-08-27
Is there any idea?
(CID:148343246)
This question is closed for comments. You're welcome to start a new topic if you have further comments on this issue.
Discuss challenges in energy and automation with 30,000+ experts and peers.
Find answers in 10,000+ support articles to help solve your product and business challenges.
Find peer based solutions to your questions. Provide answers for fellow community members!