43521members
218113posts

Connect Ecostruxure it using DCE

Cadet

Connect Ecostruxure it using DCE

First i had a connect to EcoStruxure IT using DCE. That works fine. Then i tried the free offer of Ecostruxure IT Expert and now i will go back to the first configuration.

So i tried to setup a new gateway but get the message Connecting Data Center Expert is not permitted while having an active EcoStruxure IT Expert subscription

How to deal with this ?

Tags (1)
1 REPLY 1
Highlighted
Cadet

Re: Connect Ecostruxure it using DCE

Too enable the IT Expert trail will you need to disconnect the DCE from the EcoStruxure IT instance. You will be able to do that from the Gateway section under Administration. With only the gateway should you be able to run IT Expert trial.

 

Thanks
Jesper

Tags (1)