This question was originally posted on DCIM Support by tanawat on 2019-07-02
I have one side containment that has only one row and connected to the room wall when I try to adjust this in ITA but the result of the heat map and air flow calculate have distorted value.
Is there an example to do this?
(CID:146277887)
This comment was originally posted on DCIM Support by Greg Sterling on 2019-07-03
Hello Tanawat
I do not believe a one-sided cold or hot aisle containment system is currently supported in DCO or ITA so the cooling calculations may not properly handle the configuration. I'm hoping someone from dev will confirm.
Regards
Greg Sterling
(CID:146669907)
This answer was originally posted on DCIM Support by Jef Faridi on 2019-07-04
Hi Tanawat,
As Greg mentioned that would be unsupported configuration, currently in DCO it is expected that Hot/Cold Containment System should be equipped with actual equipment (such as racks, cooling units and other floor mounted equipment).
Kind regards
(CID:146670079)
This question is closed for comments. You're welcome to start a new topic if you have further comments on this issue.
Discuss challenges in energy and automation with 30,000+ experts and peers.
Find answers in 10,000+ support articles to help solve your product and business challenges.
Find peer based solutions to your questions. Provide answers for fellow community members!