This question was originally posted on DCIM Support by Banco Central Honduras on 2019-06-20
Hi,
If i turn off my Virtual Machine with my licensed Data Center Expert APP and add more vCPUs, storage and RAM to it, do i lose my activated licenses and have to add them again?
Thank you.
(CID:145850550)
Solved! Go to Solution.
This answer was originally posted on DCIM Support by Steven Marchetti on 2019-06-20
Hi,
DCE license keys are tied to the Network Interface Card's MAC address. As long as you've not changed the card, MAC address, or re-deployed, the license keys should not be affected. Adding CPUs or RAM does nothing to the keys. If you're adding hard drive space, make sure you add an extra drive and no not increase the size of any existing drives. This will not have any affect on the license keys but will not actually increase storage as the VM has already allocated the space it will use on the drive(s) that exist.
Steve
(CID:145850553)
This answer was originally posted on DCIM Support by Steven Marchetti on 2019-06-20
Hi,
DCE license keys are tied to the Network Interface Card's MAC address. As long as you've not changed the card, MAC address, or re-deployed, the license keys should not be affected. Adding CPUs or RAM does nothing to the keys. If you're adding hard drive space, make sure you add an extra drive and no not increase the size of any existing drives. This will not have any affect on the license keys but will not actually increase storage as the VM has already allocated the space it will use on the drive(s) that exist.
Steve
(CID:145850553)
This answer was originally posted on DCIM Support by Banco Central Honduras on 2019-06-25
Thank you Steve.
(CID:145851904)
This question is closed for comments. You're welcome to start a new topic if you have further comments on this issue.
Discuss challenges in energy and automation with 30,000+ experts and peers.
Find answers in 10,000+ support articles to help solve your product and business challenges.
Find peer based solutions to your questions. Provide answers for fellow community members!