Can i add ACRC602 to an existing ACRC502 hot aisle group?
Hi Eitan,
From the modeling point of view (in DCO/ITA) it is possible to add different type of cooling units to the existing setup, eg. you can place ACRC602 to the same row as ACRC502.
Are you unable to add your cooling equipment (ACRC602) to the floor? can you please share images illustrating the issue or what you wish to achieve.
Kind regards,
Jef
Thank you for the reply,
I am asking from a physical point of view. Can those two models work together in HOT AISLE group?
Hi Etan,
It is not possible to run these two unit in the same group from a Firmware perspective,
but from the hardware side Cooling capacity and Airflow it could be done.
Kind regards,
Jef
Discuss challenges in energy and automation with 30,000+ experts and peers.
Find answers in 10,000+ support articles to help solve your product and business challenges.
Find peer based solutions to your questions. Provide answers for fellow community members!