Discuss challenges in energy and automation with a global network of peers.

39794members
181071posts

Which EDC task should I use to Extract/Load data for PME?

Schneider Alumni (Retired)

Which EDC task should I use to Extract/Load data for PME?

There are several EDC tasks available extract and load data into PME servers.

The following table illustrates the relationship between the PME version and the appropriate EDC task, along with information as to the source or destination table (datalog or datalog2) for the values.

EDC PME Tasks by PME Editions.PNG