Discuss challenges in energy and automation with a global network of peers.

39808members
181095posts

Service Tasks User Guide Version 1.15

Schneider Alumni (Retired)

Service Tasks User Guide Version 1.15

This document describes:

  • What are the Service Tasks within the Energy Data Connector (EDC)
  • The functionality offered by the different service tasks
  • How to configure the different service tasks
  • It covers the following service tasks:

               - Copy Files

               - Delete File

               - Email Upload

               - Energy Operation Start Job

               - FTP Downloader

               - FTP Uploader

               - HTTP Uploader

               - Job Stopper

               - Move File

               - PowerShell Script processor

               - Unzip Files

               - Zip Files

4 REPLIES 4
Highlighted
Lt. Commander

Re: Service Tasks User Guide Version 1.15

Hi,

I was wondering if it's possible to have a "FTP Post process settings" configuration, just like Vizelia xml task has for the uploader tasks, so you can have in different folders what is yet to be sent and what has already been sent.

Thanks

Highlighted
Schneider Alumni (Retired)

Re: Service Tasks User Guide Version 1.15

Actually yes. The current released version (v1.13) already includes the "Email Uploader", "FTP Uploader" and "HTTP Uploader".

The next EODC release (v1.14) will include more goodies like Delete/Move/Zip the produced file independently of the Load task you are using.

I do not want to write here any date, but v1.14 will be released soon.

Regards,

Highlighted
Lt. Commander

Re: Service Tasks User Guide Version 1.15

Hi Carles,

I'm not sure if you understood what I meant is that it would be good that those tasks include some post processing like vizelia Upload task:

3443

If that's what's going to be available, then that's great

thanks!

Highlighted
Schneider Alumni (Retired)

Re: Service Tasks User Guide Version 1.15

No, definitely I didn't understand your question.

The answer is yes, the new version (v1.14) will include the kind of post processing you are requesting.

3444

No release date yet, but soon.

Regards,