New in the Community? Get started here

Schneider Electric Exchange Community

Discuss and solve problems in energy management and automation. Join conversations and share insights on products and solutions. Co-innovate and collaborate with a global network of peers.

Register Now
EDC Forum
cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 
Highlighted

EDC V3.13 Hotfix 1 has been released

EDC version 3.13 (build 3.13.76.1)  has been released.

 

This new version  has 2 bug fixes. Please read the release notes before installing.

 

 

You can download the installer below. 

Tags (2)
7 REPLIES 7

Re: EDC V3.13 Hotfix 1 has been released

Hi @sesa88318_bridg, I am using this version (3.13.76.1) and I can see that the task is not showing any error, but when I get into the tabular report for PME I can see that the only data inserted was for the first meter configured, and the rest of the meters are showing the value of 0. Could you please assist?

Re: EDC V3.13 Hotfix 1 has been released

Can you attach a sample data file you are trying to import?

Re: EDC V3.13 Hotfix 1 has been released

Sorry, I though It was attached. All in the zip file

Lieutenant JG

Re: EDC V3.13 Hotfix 1 has been released

HI,

 

Thanks for providing the info and job, i'll take a look into this and get back to you.

Thomas

Lieutenant JG

Re: EDC V3.13 Hotfix 1 has been released

Hi,

I have been able to reproduce this issue and have created ticket: https://servicedesk.ems.schneider-electric.com/projects/EAS/issue/EAS-10080

 

I will revert back once I have status update.

 

Thomas

Re: EDC V3.13 Hotfix 1 has been released

Hi @sesa242992_brid ,

 

Is there any update on this?

Lieutenant JG

Re: EDC V3.13 Hotfix 1 has been released

Hi @raul_azzo_com_a 

 

I have feedback from developers...

 

Only the stream,MSB7.2_MtrdBus_NMI_6102024086
Real Energy Into the Load Interval
(kWh), which is mapped from KWH_Export, it has values in the source file. All the other ones are mapped from KWH_Import, In the source file, those streams' value are real 0s. 

 

Thomas