42489members
216105posts

Where can a replacement battery for a MicroNet LCD (Low Cost Display) be purchased

Where can a replacement battery for a MicroNet LCD (Low Cost Display) be purchased

Issue

Replacing battery

Product Line

Satchwell Micronet

Environment

  • Panel
  • Wall mounted
  • Controller mounted

Cause

Obsolescence

Resolution

Updated June 2019
The MicroNet 50 series range MN350, 450, 550, 650 LCD and Touchscreen have been withdrawn from sale.
The IAC 420, 600 and Touchscreen have now also been withdrawn from sale.
No direct replacement is offered.
Further information on these changes can be found in PA-00495 - Notice of Withdrawal - Satchwell Sigma and PA-00528 - End of Commercialization - Satchwell Sigma.

----------------------------------------------------------------------------------------------------------------------------------------------------------

Battery part number

Type LS14500

The battery is available from RS Components

Tags (2)
Labels (1)
Attachments
No ratings