Issue
What 10k Thermistor sensors are compatible with the I/A Series MNL and MNB families of controllers?
Environment
I/A Series LON Controllers (MNL-xxxxx)
I/A Series BACnet Controllers (MNB-xxxxx)
Cause
Specification information
Job spec requires a specific family of sensors. Need to know how to compare the TC curves.
Resolution
Compatible sensors that have a built-in 11k shunt resistor include the TS-5711-850, TS-57011-850, TS-57031-850, and TSMN-90110-850 Series.
Any sensor that matches resistance to temperature curve for a 10K Thermistor Type G (U.S.Sensor), Type 9 (Dale/Vishay) or Type III (ACI Series AH) can be used with the I/A Series MNL and I/A Series MNB series controllers, provided that a 11k ± 0.1% 1/8 watt resistor is wired in parallel with the sensor.
The input has a range of -10 to 135 °F (-23.3 to 57.2 °C) with an accuracy of ±1% of span.
Temperature Deg F (Deg C) |
Resistance |
Resistance Incl. 11k Shunt |
---|---|---|
32 (0) | 25490 | 8,012 |
68 (20) | 12,260 | 5,798 |
75 (25) | 10,000 | 5,238 |
104 (40) | 5,592 | 3,707 |
140 (60) | 2,760 | 2,206 |
The full temperature / resistance table for the US Sensor 10K Thermistor R-T Curve Type G sensor can be found here. Please note that the controller may not be able to use the full temperature range shown in the table.