Issue
How to search for points, names, or descriptions in SmartStruxure.
Environment
- Workstation
Cause
The SmartStruxure search feature can be performed on an entire database or on individual controllers / folders. This can help reduce the amount of time it takes to locate multiple points when creating mirrored points.
Resolution
How to search for specific names in SmartStruxure
-
Right click on the folder, object, or controller you would like to search in and click "Search. Note: When the search is narrowed down to specific areas of the database it will be able to complete the search faster than performing a full database search."
-
In the search field type in the name that you are looking for. In this example the search is for nvotemp*. This will locate all points underneath the controller that begin with nvotemp in the point name.
-
After a few seconds, depending on the size of the search area, the results will be displayed in the window to the right.
-
In order to filter the search further, click on "Advanced settings" under the search field to set more search parameters.