Issue
Embedded WebStation client licenses were needed when logging directly into a SmartX server as of 3.0.1 but are no longer needed
Product Line
EcoStruxure Building Operation
Environment
- Building Operation Webstation
- Building Operation Smartx Server
Cause
The license requirement is being removed due to market feedback. The quantity of the direct web connections to the SmartX server is restricted by the Architectural Guidelines only
Resolution
The change is available via a Hot Fix to version v3.0.3 and will be incorporated into Maintenance Release v3.0.4. In both the HotFix and the Maintenance Release, license status presentations in Device Administrator and Control Panel will indicate the availability of 99 client licenses. However, the supported quantity of direct web connections to a single SmartX server is established by the Architectural Guidelines; currently, the maximum is five concurrent connections. In v3.1, Device Administrator and Control Panel will not list client license availability at the SmartX server level since it is not constrained by licenses.