Issue
A method is needed to automatically schedule and run Continuum standard reports
Environment
- Continuum
- Windows XP
- Windows Vista
- Windows 7
- Windows Server 2003
- Windows Server 2008
Cause
Sites want reports to run automatically
Resolution
This information is also available by accessing Continuum Help (F1) in the Reports> Scheduling Automatic Reports section
To download a file with these instruction, Click Here
The file in the instructions were created with snapshots from Windows XP. The interface from Windows7 and Windows Server 2008 for the Task Scheduler has more features and is a bit different. See the following link for information on setting up a task in Windows7. Looked at the advanced area for setting up a by minute task.
http://www.7tutorials.com/advanced-users-task-creation-task-scheduler
Note: If you are having problems getting the report to run, try typing in the report command into a DOS prompt. This will give you immediate feedback to make sure the command you are using is getting executed. Doing this prior to using the command in the scheduler will help to get the command setup.