43546members
218143posts

AS Licence Inheritance from ES in EBO 3.x

AS Licence Inheritance from ES in EBO 3.x

Issue

Clarity is needed on the new License Inheritance feature which is has come into EBO from 3.x

Product Line

EcoStruxure Building Operation.

Environment

  • Building Operation Enterprise Server
  • Building Operation Automation Server (AS-P, AS-B)

Cause

The evolving Licensing Model of EBO has offered the option of Embedded Licenses in AS, such as SNMP Licenses, since EBO 2.x. 

The concept of Inheriting Licenses from an ES into an AS is a new option which can be used from EBO 3.1 onward, although the original embedded AS License option still remains, but what does this actually mean?

Resolution

In EBO 3.1, SNMP Licences may be inherited from an ES into any AS.
For an EBO system with 1 x ES and 10 x AS, the ES would only require 1 x SXWSWSNMP00001.

In EBO 3.2 SNMP and TimescaleDB. Licences may be inherited from an ES into any AS in the same manner.

Tags (1)
Labels (1)
No ratings