Learn about the Community. Join our Core Community to Get Started

Schneider Electric Exchange Community

Discuss and solve problems in energy management and automation. Join conversations and share insights on products and solutions. Co-innovate and collaborate with a global network of peers.

Register Now
Ask Exchange
cancel
Showing results for 
Search instead for 
Did you mean: 
Crewman

SQL Server 2014 SP3 supported in Continuum?

Hello

 

I have continuum 2.03 running with SQL Server 2014 SP2 but I am having problems with memory management in SQL Server. According to Microsoft release notes in SQL Server 2014 SP3, it corrects this and other issues related to SQL Server performance.

Can I update SP3 without running problems in continuum?

Tags (1)
3 REPLIES 3
Administrator

Re: SQL Server 2014 SP3 supported in Continuum?

Hey @GURBMEND , I think @CraigEl  may help you with this one

 

Oma - Your Community moderator
Crewman

Re: SQL Server 2014 SP3 supported in Continuum?

@Omaelkabili  Thank You.

Highlighted
Administrator

Re: SQL Server 2014 SP3 supported in Continuum?

Dear @GURBMEND 

 

As per the Continuum software compatibility matrix the tested and supported versions of Microsoft SQL are MS SQL2008 (SP3), MS SQL 2008 R2 (SP2) MS SQL 2012 (SP2), MS SQL 2014 (SP1), MS SQL 2014 (SP2), MS SQL 2016 SP1 Standard & Enterprise Editions.

 

2014 SP3 is likely to work, but it is untested and therefore not supported. We have not heard of any issues from the field with Continuum on SQL Server 2014 SP3.

Please make sure to take a FULL backup of the ContinuumDB before applying any patches or updates.

 

In future please post Andover Continuum related questions in the Andover Continuum forum so that your question is seen by the right audience.