43395members
217902posts

Flow Balancing on MNL controller

Highlighted

Flow Balancing on MNL controller

What software can I use to do Flow Balancing on MNL controller? I try using Workplace Tech 5.2 with Echelon USB 10 but cannot detect the MNL controller.

Tags (1)
2 REPLIES 2
Highlighted
Administrator

Re: Flow Balancing on MNL controller

Generally we use the MNL Flow Balance software. Please see the following Knowledge Base articles that refer to issues using the Echelon U10 USB LON adaptor.

 

Using an Echelon U10 USB interface function with the MicroNet VAV Flow Balance program (revision 3.0...

WorkPlace Tech will not recognize the Echelon U10 USB Lon Network Interface adapter.

Tags (1)
Highlighted

Re: Flow Balancing on MNL controller

Thanks for the sharing articles. I have done the steps but still facing the same issue. Maybe because I'm using Workplace Tech 5.2 version.

 

For the  MNL Flow Balance software, where can I find the software? Is it a license software?

Tags (1)