43195members
217453posts

Detach AS from ES

Detach AS from ES

Hello,

 

I'm trying to detach an AS, but there is no detach option available. What can I do?

 

Thanks

Kind regards 

Andries

2 REPLIES 2
Highlighted
Administrator

Re: Detach AS from ES

Hi @andries_cas-hva 

 

In order to get the correct visibility for your question you should post it in the Ecostruxure Building Operation forum.

 

You don't mention what version of EBO you are using but from the screenshot it looks like 1.x. Webhelp has the procedure to detach a server.

 

You will need to login to the AS and then from the Actions menu, point to Advanced and then click Detach server.

 

 

Highlighted

Re: Detach AS from ES

Hi @CraigEl ,

 

Thanks for the reply, but the problem is solved. The AS wasn't correclty restored.