43451members
218007posts

Can I give 400VAC supply to the motor rated of 415VAC?

Highlighted
Cadet

Can I give 400VAC supply to the motor rated of 415VAC?

 
1 REPLY 1
Highlighted
Janeway

Re: Can I give 400VAC supply to the motor rated of 415VAC?

Have to say that a motor may be out of my knowledge, but many times you could check in the datasheet, the nominell voltage for the supply if given, but also a procent over and under voltage that they specify.