42270members
186184posts

Backup set is off a different server type -SBO 2.0 unable to restore

Highlighted

Backup set is off a different server type -SBO 2.0 unable to restore

I am facing this "Backup set is off a different server type"

 

I am running on SBO2.0 & the back up file is 1.9.

I dln't think that is any issue.

 

Need assistance to solve this problem.

2 REPLIES 2
Highlighted
Administrator

Re: Backup set is off a different server type -SBO 2.0 unable to restore

Hello @nizar_iannai_co , I add @Benji to this thread, he should be able to help you! 

 

PS: do not hesitate to check the Knowledge base & use the global search bar to see if your issue was already raised before 😉

 

Oma
Global Community Manager
Community user guide  |   FAQ

Highlighted
Administrator

Re: Backup set is off a different server type -SBO 2.0 unable to restore

Hi, both server type and version (first three numbers) needs to match in order to be able to restore a backup.

 

Check the backup with the SBO xbk Analyzer - that will show you the exact server type and version. You can post a screen shot of the main dialog in the tool when you open the backup, then we can indicate which server and software you need.