Invite a Co-worker
Send a co-worker an invite to the Exchange portal.Just enter their email address and we’ll connect them to register. After joining, they will belong to the same company.
Send Invite Cancel
79290members
343968posts

xs 1500 - can't select sensitivity

Solved
mattkime0_apc
Cadet
0 Likes
1
69

xs 1500 - can't select sensitivity

This was originally posted on APC forums on 12/31/2015


i have an xs 1500 that i replaced the batteries in. when turned on, it runs the self test and then the "on battery" light stays lit and the "On Line" battery is out. i've tried to adjust the power sensitivity mode but it doesn't seem to enter the selection mode. i've tried resetting the unit as well (unplug, disconnect battery, press power button for 10s...)

any advice? 

Tags (3)

Accepted Solutions
BillP
Administrator Administrator
Administrator
0 Likes
0
69

Re: xs 1500 - can't select sensitivity

This reply was originally posted by Tom on APC forums on 1/1/2016


Hey Matthew,

What do you know about the site power? Is it normal bad? could you meter the outlet that you are plugging the unit into to make sure its getting the proper voltage. To better help you it would be great if you could provide the model and serial number of the unit. (located on the back or bottom, on a white sticker). 

Tom

See Answer In Context

1 Reply 1
BillP
Administrator Administrator
Administrator
0 Likes
0
70

Re: xs 1500 - can't select sensitivity

This reply was originally posted by Tom on APC forums on 1/1/2016


Hey Matthew,

What do you know about the site power? Is it normal bad? could you meter the outlet that you are plugging the unit into to make sure its getting the proper voltage. To better help you it would be great if you could provide the model and serial number of the unit. (located on the back or bottom, on a white sticker). 

Tom